This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA128输出不稳定

Other Parts Discussed in Thread: INA128

用仪表放大器放大压力传感器输出mV信号(-15mV-15mV), 放大200倍,现在的问题是:

1.输出AV1不稳定,漂移在0.3V左右。不知何原因?

2.V+,V-没有接0.1uF的电容,不知影响大不?对正负5V的要求纹波多大??

3.需要考虑电源屏蔽环吗,如何设计?

4.IN128A输出要并并联51K的负载电阻不?

5.只有R2,R3用了0.02%的精密电阻,其它用普通2%电阻,这个重要不

附件为INA128原理图,请各位大侠们指导!