This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
查了一下S6968的pdf,它的偏置电压加到12V时,结电容达到30pf。按照你给的图,跨阻取100K,电容取10u,仿真了一下,系统3db带宽1K Hz都不到。把电容换成0.1p,3db能达到10多M Hz。
你好·,刚刚的图形有点问题。用的是跨阻100K,电容是10PF。准备用您说的0.1PF试一下。想问一下,您用的仿真软件是哪一款?如何测试3DB带宽?
我用的是和你相似的图,你的Va电压是多少,我用的是12V,出来效果和你相似,我采用了两级运放。
我在用OPA657作为光电转换的前置点电路的同时,也用OPA657搭了一个功率放大器,我看示例中并没有特别的备注,需要注意什么。除了加去耦电容
你好,昨晚打板测试,电容用的是10PF,但是还是没有信号输出。请问,原因可能是哪方面呢?另外,可以教我如何用tina仿真3DB时的带宽吗?