www.deyisupport.com/.../12166.aspx 上面帖子是前些日子请教的问题,感谢你的答复,OP的上面和输出部分我都能理解,上面是反相求和,输出加RC防止自激,但你有提到OP的正向输入点需要加入基准电压,这怎么理解呢?我没找到相关资料,烦请传授下;另外这个输出是反相的-3.25v~-50mv,你为何说是输出范围是58mv~3.25V呢?感谢,期待回复~~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
www.deyisupport.com/.../12166.aspx 上面帖子是前些日子请教的问题,感谢你的答复,OP的上面和输出部分我都能理解,上面是反相求和,输出加RC防止自激,但你有提到OP的正向输入点需要加入基准电压,这怎么理解呢?我没找到相关资料,烦请传授下;另外这个输出是反相的-3.25v~-50mv,你为何说是输出范围是58mv~3.25V呢?感谢,期待回复~~
1. 因为你的信号是0到5V的,里面有两部分,一是2.5V的直流成分,不随时间变化;二是+/-2.5V的交流成分,随时间变化。你想得到的是0到3.3V的输出,这里面不仅有+/-1.65V的交流成分,还有1.65V的直流成分。所以需要在正端加个基准电压,把2.5V的直流成分搬到1.65V去。
2. 同相反相都用正的电压幅度表示,应该没啥问题吧?另外,58mV到3.25V是仿出来的,因为365的摆幅不能压到GND,离GND还有20~30mV,所以保险起见,把最低摆幅稍稍抬高一点,避免输出超过芯片额定的范围。
2.5V+/-2.5V只是针对MLX91205吧?如果我用其他的输出就不一定是这个范围了应该,比如下图的,我同样通过外部LM393比较器芯片输出的模拟信号来通过OPA2365给MCU的AD模块,也需要这样的基准配置吗?我有测试过LM393在正常供电情况下输出是5V的,在光线摆动情况下,最低会跌落0V,这样的输出模拟电压也会是以2.5V为分段一部分为直流,一部分为交流吗?thanks~~
1. +/-2.5V是针对MLX91205的。实际应用中,需要你自己去调那个直流基准。比较稳妥的办法是先对信号做直流分析,把各个电压节点的直流工作点确定好,然后再做交流分析。做交流分析时,直流偏置和基准电压可以看成交流地。
2. LM393是个比较器,输出电压已经是个数字量了,可以直接进MCU处理的(或者经过一个电平转换再进MCU),为什么还要对比较器的输出做AD啊?
1.那2.0V的基准是你随意给的喽,只是因为是3.3所以降低了2.5V基准为2V,是吧,我以为是OP的一个标准什么的呢~
2.LM393输出是5V的,原本我想同样通过OPA2365输出给AD,上次有跟你说是6个通道,可能是2个MLX91205的,4个通道就是393出来的信号;这样可以统一一点,但好像成本有点高,有可靠的电平转换芯片推荐吗?
非常感谢你~~
1. 不是随便给的,要调出来的。不是一个OP的标准,只是为了直流工作点正确,加上去的。
2. 你要5V转多少V?3.3还是1.8?
明白了,非常感谢~~
5V转3.3的,有双通道的更好~~
你先评估一下SN74LVC2T45,双路电平转换,1.65V到5.5V,正好能覆盖你3.3V到5V的应用。数据率最高能跑到420M,也应该满足你应用了。同时,也可以去官网找找。
早期时候没有想到用OP,因为OP用的少也生疏了很多;那会一直想找颗level shift的芯片来完成,
这么说的话,电平转换同样是可用于MLX91205的喽?我这么理解没有错吧?谢谢~~
要是用电平转换的方案,等于说你把模拟信号的数字话放在MCU之前了,那么MCU接收的就是一个1 bit的比较器输出,至于这个精度够不够你应用,你可以再去评估一下。如果用365的方案,等于说数字化是发生在MCU内部的ADC里,精度会高一点,也需要你再去评估一下。
感谢~~~整体还是用2365吧,对于其他的模拟信号输出芯片,我再做相应的调整基准电压就好了~~