This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA333输出电压

Other Parts Discussed in Thread: OPA333

电源为5v-0,v +为5V,v-连接到地,我的电路图在下面,IN +连接到0-5V电压源,IN-连接到2.5V。可以得到-2.5V到2.5V的 输出吗?

  • 不可以

    运放不可能输出比 VSS 更低的电压, 这时候内部电流工作在非线性的饱和状态

  • 可以看下OPA333的输出电压范围。Voltage output swing from rail典型值为30mV,也就是说单电源5V供电的话,输出范围最大为30mV~4.97V. 不可能输出负电压范围。

    建议选择双电源供电。

x 出现错误。请重试或与管理员联系。