This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

詢問LM339遲滯電路-當輸入快到下限電時,輸出產生彈跳現象?

Other Parts Discussed in Thread: LM339

输入您的问题

請教個位前輩是否有遇到這個問題~
下圖為遲滯電路,作為電池過放電壓後切斷LOAD功能,請參考圖一
以下設計VTH=10.8V   VTL=9.8V   VREF=10V
VBAT_OP為電源12VRY-BAT為電池電壓
 
電路動作原理:RY-BAT電池電壓低於比較電壓D12--10V時,輸出OPALO
 
問題出現:輸出暫不接LOAD,當RY-BAT快到下限電壓9.8V時,輸出會產生彈跳現象(約1.5秒),直到低於參考電壓才關掉         (請參考圖二波形圖)                                   
  (圖一)
 
                       
           

緣色波形:VBAT_OP(LM339電源)
黃色波形:OPA輸出T8
藍色波形:電池電壓T6
紅色波形:參考電壓T7
產生雜訊處為OPA輸出快OFF時,約1.5SOFF
(圖二)