我准备用正负24V供电,LM3886的供电电流应该多大
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
供电电流是和负载有关的,我想您参考这个参数,是想看带载能力吧,那么在选择power时候,power IC datasheet中会对输出电流有描述。
我得知道这个LM3886在工作的时候他需要多大的电流才能驱动, 我才能选择合适的电源芯片给他供电。LM3886手册figure6图像描述了在输入正负24V时,supply current在50ma附近,那我选择一个输出电流在100ma以上的电源芯片不就行了吗?
亲;LM3886是功率放大器;是可带功率输出的。除非亲只用作电压放大;负载电流小于20mA,亲的决定才是可接收的。
举个实例吧:
假设LM3886带4欧负载,24V供电下的最大电流;实际上就是攻防饱和输出时的负载电流。可以粗略的计算为:
24V除以4欧,等于6A。也就是说,亲需要为LM3886准备最大6A输出能力的电源才刚刚够用。
由于6A远大于50mA电流,这静态电流就忽略掉了。
假设负载是10k,24V供电下的最大负载电流是:24V除以10k;等于2.4mA。那么;亲需要提供的电流为:
50mA+2.4mA=52.4mA
所以;亲在决定前;必须弄清楚负载究竟是多大,否则;差以毫厘谬着千里。