Other Parts Discussed in Thread: AMC1200
我的产品是10个5V输出并联,50v输出,我想测每个产品的电压,选择amc1200。由于产品比较多,不想再输出端增加运放以减少成本,如下图。不知道可以吗?隔离电压为B0505s模块,不知道电压波纹会对检测有影响吗? 我的检测精度要求不高,0.05V误差就可以。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
问题1:在精度要求不是很高的情况下,输出测VOUTN(6脚)和GND(5脚)可以直接连接在一起吗?作为单端输出接入模拟开关,然后给单片机ADC。
精度要求不高的情况下,也不能将输出VOUTN和GND接在一起,因为输出有共模电压,必须用一个运放实现差分转单端的功能。如果需要,电路可以推荐给你。
问题2:我检测5V,左侧供电3.3V是否可以?
可以,只要保证输入信号范围在+-250mV范围内。
Hi hao,
建议在AMC1200电源管脚加足够的去耦电容;然后断开R15,R19,隔断AMC1200与后级电路的连接来测量AMC1200的输出,首先确保AMC1200的输出正确。