电路图如上,通电后,只能实现+10V的输出,应该-10V的输出确实-9.2V,是电路的问题吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
没太理解您的问题,同相端ADCINA接的是地?
“只能实现+10V的输出,应该-10V的输出确实-9.2V” 什么意思?
不好意思啊,我好像没描述清楚,是这样的,电路如图,这是一个将DAC的0~3V的输出放大为-10~+10V的电路。我在通电后,让DAC输出3V的电压,在运放的输出端可以得到+10V的电压,但是我让DAC输出0V的时候,在输出端得到的电压却是-9.2V,我检查了电路和DAC输出端的电压没有问题,所以怀疑是不是器件选型的问题
你好,
按照电路的参数计算,0V时,对应的输出电压为-13K/2.4K×1.76=-9.5V,是达不到-10V的
你好,
根据电路参数计算确实无法得到-10-+10V输出,但是可以通过将偏置电压设为1.77V,并且将R2阻值改为2.3K实现.