This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CD4013电路问题



采用CD4013(CD4013BM96)作为按键开关电路,

发现有如下的问题,第一步将Q1后级的R1 MOS管都去掉,第二步,采用3.3供电,用万用表测试Q1发现始终为高电平,无法切换。 但是测试 Q1非 引脚,发现可以切换,(仅仅是在万用表测试电压档正极挨着Q1非 引脚的时候电路 Q1才可以正常切换)

随后发现拆掉C4电容后 在3.3v下可以实现Q1的电平切换。

但是发现4.2v不可以,随后用万用表测试,发现万用表接到q1非 线上时,如果为x1档,电路可以正常切换,如果为x10档则电路无法工作。

对Q1非线电路进行 上下拉均无效。

请帮忙解释一下。

  • 亲,这个电路有许多问题。

    首先;由于CD4013集成的是同步触发,所以;它对时钟沿有要求。你的RC输出沿不够快,无法使用。

    其次;输出开关需要续流。电子开关有它自身优势和弱点。不能简单替换。