这个电路的电压转电流如果使用LM358A可以正常工作,如果使用OP2277与TL082的时候不能输出低于7ma电流。请教一个跟那个参数有关,如何调整?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
输出电流不能低于多少,说明还是指的输出电压不能低于多少,因此也就是衡量的运放输出的最小电压值的问题。
LM358A单电源供电时,Vol可以看到最大20mV,典型值为5mV,近乎零电压轨了。 对比一下,其他两款最低电压就要大很多了,因此也就是输出电流不能低于某个值了。
另外,TI有专门的4~20mA的transmitter,可以参考一下www.ti.com/.../products.html Transmitter