用OPA656做了个减法器电路,OPA656芯片是正常的,我用信号发生器发出信号,电线接到运放的输入端,然后输出就出现了一堆乱七八糟的波形,但是如果先经过一个别的运放跟随一下信号,再接到OPA656,减法器就正常工作。怀疑是我用的电线比较长?(不到1米)导致电线上的电感和OPA656产生了谐振。
从网上查找解决谐振的方法,说在反馈电阻上并联一个pF级的电容,我并联了一个5pF的,但是没有效果。
请教一下大神们到底如何解决这个问题
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想弄清楚的关键问题是,究竟怎么调参数才能解决这个问题,例如说改变反馈阻抗,或者在输出加电容等方法。如果按目前的结论,是线长导致的,那么我把线改短一半是不是就不会出现这种情况了?如果还会出现,那究竟多短才不会出现这种情况。论坛里关于OPA656的问题全部都是基本电路发生谐振,那么就说明OPA656里面有大家忽略的因素存在导致了谐振
PCB设计是很容易被大家忽略的一个问题,OPA656不像OP07、LM358那样差不多的设计都可以正常工作。OPA656带宽达到500MHz,输出容性带载能力非常低,不注意设计就会造成器件震荡,输入端的电容也要非常注意,手册中指出了多条注意事项,建议仔细阅读数据手册。