This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
看网站TI功率放大器工作频率都比较小,功率驱动负载也比较小。
我们需要一款工作频率在500KHz,驱动负载在200Ω以上,功率在20W以上,不知道有没有这样的功率放大器
你好!
可参考:
OPA541 - 80V supply with 10A continuous output
OPA544 - 70V supply with 2A continuous output
选型参考:
http://focus.ti.com/paramsearch/docs/parametricsearch.tsp?family=analog&familyId=1483&uiTemplateId=NODE_STRY_PGE_T
这两个好像频率在500K时,电压增益系数很小了。
可以先放大信号,然后送至OPA
你意思是先用三极管放大搭一个放大电路,放大500KHz交流信号后,在1:1给功率放大器放大输出
可以做两级放大,THS3001 +OPA541