Other Parts Discussed in Thread: ISO124
使用多个iso124隔离电机控制信号,每个ISO124的输入输出电源是否都需要独立?即若24V电源输入,需要±12V给ISO124供电,是否需要12个稳压模块分别给ISO124供电?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ISO124
使用多个iso124隔离电机控制信号,每个ISO124的输入输出电源是否都需要独立?即若24V电源输入,需要±12V给ISO124供电,是否需要12个稳压模块分别给ISO124供电?谢谢!
十分感谢!我重新看了电机输入要求:“各电机的信号电源(12V)需要相互隔离,各电机的控制信号(±5V模拟信号)需要相互隔离,信号电源与信号共参考地”。所以我使用iso124来隔离控制信号,又用了12个稳压模块(±12V)分别给6个iso124的输入输出供电,又用了6个12V稳压模块给电机信号电源供电(信号电源地和主地没有连接)。所有的iso124输入电源地都分别通过0Ω的电阻和主地相连,所有的iso124输出电源地都分别通过0Ω电阻和6路电机信号电源地(不知道这样算不算满足共参考地的要求...)。然而又查看了iso124的数据手册,发现在典型工作电压(±15V)下最小输入电压是±10V,这样看当工作在±12V时,输入电压范围也不可能降到0V,肯定不满足条件。这样说iso124不符合?(不知道怎么贴图,抱歉,再次感谢您的回复)