This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
采用OPA551设计电路,在进行65℃高温工作时,发现该芯片的flag引脚出现告警提示,与器件手册信息不符合,希望能提供帮助,确认问题点:
电路设计如下:
常温条件下测试,flag电压(即R637端电压)从0.3V缓慢上升到1V左右,后续拆掉U70芯片测试,此处电压变化相同。
高温工作试验时,运放空载,无负载电阻。
结合高温工作的记录数据,绘制曲线如下:(横轴是测试点,不是时间)
希望能确认OPA551的flag输出设计是否如此,当前测试到的状态是正常,还是故障?
您好,flag引脚告警预示的温度160度指的是芯片的结温,不是操作温度。
所以当温度升到65度的时候,您测量下流经电源的电流是多少,然后计算下功率。然后根据热阻计算下结温是否超过160度就知道flag告警是否正常了。
参考OPA551 datasheet 10.3 power dissipation部分的计算公式:
输出是空载,没有负载电流,芯片设计是±15度供电,根据计算65℃环境温度时,结温是79°,没有超过芯片的设计温度。从资料看,我认为flag引脚输出的电流应该是阶跃的,正常<50nA,告警时80~120uA,从实际测试数据来看,好像是随温度连续变化的,不知道连续变化这种情况是不是芯片的正常状态?!