Other Parts Discussed in Thread: OPA2188, OPA2333, OPA188
您好,我下载了slau502.pdf文档,里面的仿真图如下:我用opa2188替换opa2333,Vcc改成24V,为什么就实现不了镜像电流呢?输出已经不在是100mA,请问是什么原因呢?非常感谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
感谢您的回复,我附上slau502.pdf里面的仿真文件,这是没有问题的,仿真也正常。恒流是100mA输出。现在我急切需要知道的是,如果将OPA2333换成OPA2188,输出是否还是100mA?换放大器的目的是因为OPA2188的供电电压比较高,这样的话我用24Vdc供电,输出的compliance voltage也比较高,驱动负载的能力也比大很多。盼复!Tina Sim FINAL_NTF2955.TSC
Hi Amy,
谢谢您的回复。我按照您的指导,重新做了一次仿真。这次仿真是将slau502.pdf里面的OPA2133换成了OPA188,同时进行了瞬态和稳态响应分析。发现稳态输出稳定,但是不再是100mA的输出电流。我的原理分析是这样:U1 OPA188 同相端输入+2V,根据虚短反相端也就是V_Rs1+2V,I_Rs1就是1mA,这样的话U2 的同相端是5-0.47V=4.53V,根据虚短U2的反相端是4.53V,这样的话理论上I_load=(5-4.53)/4.7=100MA,一个完美的镜像电流放大输出。但是仿真结果输出是大约是110mA,而且U2的同相和反相端电压不相当,不知道什么原因?想请教一下,同时附上了仿真文件方便您验证,谢谢了。100MA OPA188.TSC
原因找到了,是放大器输入和供电范围引起的。从仿真结果看,opa188放大器似乎不是rail to rail输出,但是datasheet明确说是rail to rail。不知道为什么?不过这不影响我的使用,再次感谢。