我用PGA280+AD7765进行信号采集。
发现只有AD7765输入端短接,噪底很低。但是PGA280+AD7765一起测试,输入端短接的时候噪底很高,请问是为什么啊。
下面是原理图。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
PGA280是一种可编程增益放大器,用于直流精密测量,通常用于相对低频信号。它通常与输出数据速率相对较低的delta-sigma转换器配对使用,测量低频范围内的信号或直流信号。下图是增益为1的PGA281的总噪声TINA仿真图(PGA281与PGA280使用相同的核心放大器)。在上述电路配置中,增益为1V/V时,PGA280的预期总输出噪声为@1MHz,136uVRMS(或约0.9mVp-p)。
系统上的总噪声也将取决于delta-sigma转换器数据速率和数字滤波器设置。例如,在输出数据速率为~156kHz时,AD7765的数字滤波器指定-3db带宽为64kHz。在此频率下,PGA280的噪声预计约为59.8uVRMS(或相当于~0.4mVp-p),与您测出的0.5mVpp也比较接近了。降低噪声的一个建议是降低Delta-sigma的数据速率或减少Delta-sigma数字滤波器设置的f(-3dB)带宽。
经过筛选,支持1、10、100增益和+/-10V电源的可编程增益放大器有PGA202和PGA103。
PGA103提供单端输入,噪声密度为11nV/sqrt(Hz),0.1-10Hz的低频噪声为0.6uVp-p。PGA103噪声性能与增益有关,具体请查看数据手册INPUT VOLTAGE NOISE vs FREQUENCY图。
PGA202提供差分输入,噪声密度为12nV/sqrt(Hz),低频噪声为1.7uVp-p(0.1-10Hz)。请注意PGA202的允许输入共模电压是自电源轨VCC-5V。
这两种PGA都提供单端输出,因此双放大器级(如OPA2320)可用于执行单端到差分转换,并将信号转换为AD7765调制器所需的2.048V共模。请参阅下面可能的电路