This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA280噪底很大问题?

Other Parts Discussed in Thread: PGA280, PGA281, PGA202, PGA103, OPA2320

我用PGA280+AD7765进行信号采集。

发现只有AD7765输入端短接,噪底很低。但是PGA280+AD7765一起测试,输入端短接的时候噪底很高,请问是为什么啊。

下面是原理图。

  • 您好,
    您输入的信号频率是多少,增益设置的是多少,可根据数据手册figure16 噪声频谱密度计算噪声,判断下PGA280的噪声性能是否正常
  • 另外,供电电源的纹波,输入输出信号是否耦合了其他噪声信号等也会影响其性能
  • 您好,我是直接把输入端短接的,没有输入信号。增益是1倍。也就是不放大。提供了一个2.048的共模电压,经过AD7765采集后噪底很高。

  • 我看了看电源波纹也不错。我直接将输入端短接还是很大噪底。

    噪底大概在0.5mv。

  • 您在哪里提供了2.048V的共模电压,有没有查看2.048V的电源性能怎样
  • 我看手册上说不需要特别精准的共模电压的,但我后来用一个专门芯片ADR440提供2.048的共模电压,还是不行。

    在精准的电压芯片也不可能完全就是2.048,最起码有mv或者uv的误差。

  • PGA280输入不需要共模电压,我刚看了AD7765的数据手册,您是给AD7765提供的输入共模电压是吗,如果是,那么您短接输入、单独测试AD7765的输出噪声时,是不是也有提供了这个共模电压?
    短接输入、单独测试AD7765时,输出底噪有多少
  • 嗯,是因为AD7765需要共模电压所以给了PGA280一个共模电压。
    短接AD7765输入端噪底要低很多。
    目前测量的是:PGA280+AD7765噪底是1200; 单独短接AD7765噪底是300以内
  • 我还测过PGA280不接共模电压,直接给AD7765,有AD7765自己提供2.048的共模电压,结果还是一样
  • PGA280是一种可编程增益放大器,用于直流精密测量,通常用于相对低频信号。它通常与输出数据速率相对较低的delta-sigma转换器配对使用,测量低频范围内的信号或直流信号。下图是增益为1的PGA281的总噪声TINA仿真图(PGA281与PGA280使用相同的核心放大器)。在上述电路配置中,增益为1V/V时,PGA280的预期总输出噪声为@1MHz,136uVRMS(或约0.9mVp-p)。

    系统上的总噪声也将取决于delta-sigma转换器数据速率和数字滤波器设置。例如,在输出数据速率为~156kHz时,AD7765的数字滤波器指定-3db带宽为64kHz。在此频率下,PGA280的噪声预计约为59.8uVRMS(或相当于~0.4mVp-p),与您测出的0.5mVpp也比较接近了。降低噪声的一个建议是降低Delta-sigma的数据速率或减少Delta-sigma数字滤波器设置的f(-3dB)带宽。

  • 您能推荐一款和AD7765配合使用的PGA吗,当然,噪声越小越好
  • 您输入信号带宽是多少呢,也是需要2对差分输入吗,还是±10V供电吗,最大增益有没有要求?
  • 带宽在10-10KHz之间,

    最好是差分信号,不是差分信号也行。

    对,±10V供电

    增益的话最好,1、2、5、10、20、100倍可调。

  • 经过筛选,支持1、10、100增益和+/-10V电源的可编程增益放大器有PGA202和PGA103。

    PGA103提供单端输入,噪声密度为11nV/sqrt(Hz),0.1-10Hz的低频噪声为0.6uVp-p。PGA103噪声性能与增益有关,具体请查看数据手册INPUT VOLTAGE NOISE vs FREQUENCY图。

    PGA202提供差分输入,噪声密度为12nV/sqrt(Hz),低频噪声为1.7uVp-p(0.1-10Hz)。请注意PGA202的允许输入共模电压是自电源轨VCC-5V。

    这两种PGA都提供单端输出,因此双放大器级(如OPA2320)可用于执行单端到差分转换,并将信号转换为AD7765调制器所需的2.048V共模。请参阅下面可能的电路