This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA400-Q1EVM程序下不进,小白求解释,谢谢。



如题,下载hex文件出现如下报错:

ERROR - OTP Progamming was NOT successful. Please check the 'Error' Tab for more information
ERROR - Register 026A, was programmed to: 22, but read back: 00
ERROR - Register 0269, was programmed to: EF, but read back: 00
ERROR - Register 0268, was programmed to: 80, but read back: 00
ERROR - Register 0267, was programmed to: A3, but read back: 00
ERROR - Register 0266, was programmed to: 0D, but read back: 00
ERROR - Register 0265, was programmed to: F5, but read back: 00
ERROR - Register 0264, was programmed to: 0D, but read back: 00
ERROR - Register 0263, was programmed to: 25, but read back: 00
ERROR - Register 0262, was programmed to: 93, but read back: 00
。。。

小白求解释,多谢了。