This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如题,下载hex文件出现如下报错:
ERROR - OTP Progamming was NOT successful. Please check the 'Error' Tab for more information
ERROR - Register 026A, was programmed to: 22, but read back: 00
ERROR - Register 0269, was programmed to: EF, but read back: 00
ERROR - Register 0268, was programmed to: 80, but read back: 00
ERROR - Register 0267, was programmed to: A3, but read back: 00
ERROR - Register 0266, was programmed to: 0D, but read back: 00
ERROR - Register 0265, was programmed to: F5, but read back: 00
ERROR - Register 0264, was programmed to: 0D, but read back: 00
ERROR - Register 0263, was programmed to: 25, but read back: 00
ERROR - Register 0262, was programmed to: 93, but read back: 00
。。。
小白求解释,多谢了。
这个是上位机软件,初始设置,没有配置。求解。
请按照EVM user's guide 中的给出步骤进行操作,参考page24 “6.6.1 Load .HEX File into GUI” 部分,看在哪个环节出现了问题 http://www.ti.com/lit/ug/sldu010/sldu010.pdf