这个是我们制作的一个采集电流的电路,电流采用隔离运放AMC1301,然后485发送数据,在实验室里,当没接入485的 A B 线时,采集的电流很准确,但是一旦接入485的AB线,电流就跳变的厉害,还有就是设备拿到现场以后,没接入485和负载时,分流器没有电流,但隔离运放再放大后 AD口采集到的电压直接是最高电压,拿了另外一个设备去现场,装上负载后,AD口采集到的电压又是0,分析了好几天也没看出问题来。大家帮忙分析下电路,是不是因为AMC1301的GND和采集端的GND没有共地呢?如果共GND的话,现场分流器之间是有距离的,多路采集时,GND和GND之间是有压差的。怎么办呢?