INA233空载时,读得MFR_READ_VSHUNT的值很大,在测量有负载时比较数值正常,是怎么回事呢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我所说的情况是没涉及负载的,你看IDC座子上什么都没接。
我重新试了一些方法:
1、将R110和R111都换成0Ω的电阻,测得VRSHUNT基本为0mv,因此我怀疑是IN+和IN-的漏电流造成的。
进一步的:
2、我将之前采样电阻从100mΩ切换到1K,此时测得VRSHUNT=6mv左右,计算出对IN-引脚约6uA漏电流;
再次如果采样电阻为10K,测得VRSHUNT=36mv左右,计算出对IN-引脚约3.6uA漏电流;
如果采样电阻100K,测得VRSHUNT=90mv左右,计算出对IN-引脚约0.9uA漏电流;
通过上面的数据我找不出规律,你看否能看出什么问题?