This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请推荐一个高边电流采样方案

Other Parts Discussed in Thread: TMCS1101

因为一些原因,开关电源的输出电流只能从高边采样。开关电源输出0到60V,电流0到10A,TI的“

High Voltage 12 V – 400 V DC Current Sense Reference
Design”方案无法在接近0V的场合工作。隔离采样成本太高,有没有更简单改价比更高的方案。谢谢了。
一、该方案采样精度需要0.1%的精度,有软件校准,因为共模电压是不断变化的,使用高共模运放线性度是否会很差而影响精度?
二、使用下图所示放大电路,运放用TI的OP07C是否可以实现
  • 可参考TI的TMCS1101系列,它们是isolated Hall-effect current sensor。输入侧不需电源,内阻小,插入损耗小、等效电阻大(从50--400mV/A)、适用于高边或低边、交直流通用。类似的还有Allegro、Magntek、Melexis等,它们都有Pin to Pin兼容的型号。
    美中不足的这类芯片的带宽不高,一半都在100KHz左右。
    FYI!
  • 看过这个器件,没试,因为看到总误差1.5%。因为精度要0.1%以内,AD采样后有软件校准后,但是校准后不知道温飘过不过得了。实在没办法时可以尝试一下。100KHZ带宽已经够用。感谢推荐。
  • 您好,

    OP07C的输入共模电压不能满足您的要求

    我看了下TI的电流感应运放,在0到10A范围没有可以做到0.1%的精度,在每个电流感应运放产品主页“Design & development”部分有Current sense amplifier error analysis工具,如下截图,被检测电流越小,误差越大,您可以考虑分段检测,比如说0~100mA采用一个采样电阻值,100mA~1A采用一个电阻值,依次类似到10A。