你好,我想咨询一下我计划进行微弱光信号检测,微弱光信号检测,高增益宽带宽,带宽大于10M,光电流pA级别,目前有以下两个方案
(1)用OPA857进行IV转换电路的运放,这个我看增益很小,反馈电阻固定20K,这么小的增益怎么实现微弱信号放大,我可不可以在流压转换后面加两级放大利用THS4541进行两级放大,甚至是三级,如何评估这个设计是否可以实现呢
(2)再有就是利用OPA855作为流压转换,利用仪器放大器进行放大,仪器放大器计划用INA849
希望大家给点指点看看是否可行
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我想咨询一下我计划进行微弱光信号检测,微弱光信号检测,高增益宽带宽,带宽大于10M,光电流pA级别,目前有以下两个方案
(1)用OPA857进行IV转换电路的运放,这个我看增益很小,反馈电阻固定20K,这么小的增益怎么实现微弱信号放大,我可不可以在流压转换后面加两级放大利用THS4541进行两级放大,甚至是三级,如何评估这个设计是否可以实现呢
(2)再有就是利用OPA855作为流压转换,利用仪器放大器进行放大,仪器放大器计划用INA849
希望大家给点指点看看是否可行
您好,pA电流输入,需要反馈电阻多大阻值,或者说要得到做大电压的输出?
几款常用大带宽的跨阻运放,比如OPA657,OPA847,OPA659等,根据您 的实际应用, 计算下-3dB的稳定带宽是多少。
附件是一篇关于跨阻运放应用指南,可以根据里面给出的公式计算下这几款高带宽的运放在-3dB下的稳定带宽。
你好,谢谢您的答复,暂定是100K,您说的这几款我计算过了在100K的化都不太满足10M的-3db稳定带宽,我用OPA657和OPA847进行过实验但是带宽不满足,甚至OPA847在20K的时候出现了很大的0点漂移(就是没有光照的时候会输出一个3.7V的电压)
所以看到贵公司的OPA855和OPA857想用这两款进行第一级放大,担心是不是满足此要求。但是后端的二级三级放大不知道如何设计,有没有推荐的运放进行二级三级放大,附件是我的电路图7180.电路图.docx