This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

微弱光信号检测,高增益宽带宽,带宽大于10M,光电流pA级别

Other Parts Discussed in Thread: THS4541, OPA857, INA849, OPA855, OPA659, OPA657, OPA847, INA166

你好,我想咨询一下我计划进行微弱光信号检测,微弱光信号检测,高增益宽带宽,带宽大于10M,光电流pA级别,目前有以下两个方案

(1)用OPA857进行IV转换电路的运放,这个我看增益很小,反馈电阻固定20K,这么小的增益怎么实现微弱信号放大,我可不可以在流压转换后面加两级放大利用THS4541进行两级放大,甚至是三级,如何评估这个设计是否可以实现呢

(2)再有就是利用OPA855作为流压转换,利用仪器放大器进行放大,仪器放大器计划用INA849

希望大家给点指点看看是否可行

  • 你好,我想咨询一下我计划进行微弱光信号检测,微弱光信号检测,高增益宽带宽,带宽大于10M,光电流pA级别,目前有以下两个方案

    (1)用OPA857进行IV转换电路的运放,这个我看增益很小,反馈电阻固定20K,这么小的增益怎么实现微弱信号放大,我可不可以在流压转换后面加两级放大利用THS4541进行两级放大,甚至是三级,如何评估这个设计是否可以实现呢

    tiduaz1.pdf

    (2)再有就是利用OPA855作为流压转换,利用仪器放大器进行放大,仪器放大器计划用INA849

    希望大家给点指点看看是否可行

  • 您好,pA电流输入,需要反馈电阻多大阻值,或者说要得到做大电压的输出?

    几款常用大带宽的跨阻运放,比如OPA657,OPA847,OPA659等,根据您 的实际应用, 计算下-3dB的稳定带宽是多少。

    附件是一篇关于跨阻运放应用指南,可以根据里面给出的公式计算下这几款高带宽的运放在-3dB下的稳定带宽。

    4718.跨阻放大应用指南.pdf

  • 你好,谢谢您的答复,暂定是100K,您说的这几款我计算过了在100K的化都不太满足10M的-3db稳定带宽,我用OPA657和OPA847进行过实验但是带宽不满足,甚至OPA847在20K的时候出现了很大的0点漂移(就是没有光照的时候会输出一个3.7V的电压)

    所以看到贵公司的OPA855和OPA857想用这两款进行第一级放大,担心是不是满足此要求。但是后端的二级三级放大不知道如何设计,有没有推荐的运放进行二级三级放大,附件是我的电路图7180.电路图.docx

  • 1nA的输入,最终输出为4V
  • 您好,如果第一级1nA输入,100K反馈电阻的话,输出只有0.1mV,如果需要输出4V的电压,那么需要运放的增益带宽积也很大,并且是输入失调电压比较小的精度运放。 INA166的仪表运放增益G=2000,但是-3db的稳定带宽为450Khz,所以也不能满足需求。
    所以第一级的放大,需要增大反馈电阻, 100K的话输出只有0.1mV,二级放大的运放型号不太好找。
  • 增大反馈电阻比如增大到1M那第一级IV转换的带宽就不够了,所以现在计划用3级放大电路,IV+一级放大+二级放大,后面放大利用差分放大电路这样能够减少误差。我想找一款能够进行微弱信号放大的差分放大器,放大倍数100倍