This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMV358: LMV358MX技术咨询

Part Number: LMV358

Hi team

Good day

客户需要获得技术支持,麻烦帮忙看下:

LMV358MX由单电源+5V供电,BREAKH和BREAKL端用来接外部电压输入,BREAKH_MCU和BREAKL_MCU接单片机AD采集口,R613和R614为NC状态。
如下两个问题:单电源+5V供电状态下,
1、当BREAKH和BREAKL端悬空时,本人测量此两端对地都有大概0.4V-0.5V的电压,问此电压来自哪里?是否为正常状态?
2、如果悬空时BREAKH和BREAKL端有电压存在,那么当BREAKH和BREAKL端不悬空并且有电压输入时,存在的电压是否会对外部输入的电压产生影响(比如将外部输入电压拉低)?

Regards

Aosker

  • 您好,

    R613和R614 NC后,且BREAKH和BREAKL端悬空时,输入端会耦合环境中的电磁干扰,那么它会存在一个潜在的输入,运放的输入端是需要避免这种状态的,因此如果运放的BREAKH和BREAKL端会有悬空的状态时,是建议加上R613和R614电阻的,这样在没有输入时,运放的输入端是一个固定的电平状态。

    当BREAKH和BREAKL端有电压输入时,其悬空时存在的电压(其实是环境中的噪声信号)对运放影响很小。

    另外,您的运放工作时是稳定的吗?因为我看到您在运放的输出端接了两个电容,这很容易引起运放的不稳定,形成振荡,因为这相当于容性负载,LMV358没有这么大的容性负载的带载能力