This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
利用OPA657搭建了一个宽带宽的积分器电路
从Bode图中可以看出在100Hz到1MHz有明显的积分效果,仿真结果也证明了这一点
但是在实际电路中,效果如下图
不知道问题出在哪里,请帮忙解决
仿真时,在输出端接一个接地电阻或者接电压跟随器时输出信号与实际波形一致(如黄色波形只有高低电平);当输出接比例为1大的反向比例运放时,可以在输出端接一个电阻然后接地,输出与理论计算一致
积分电路电容是跨接在反向输入端和输出端之间,您这个电路形式设计的就是这样的吗
看您的实际电路,输入信号经R1和C1低通滤波电路输入至运放反向输入端,而RC滤波器的截止频率大概为81HZ,输入至运放的有效信号基本上都被衰减至0了,这一点不知道是不是您需要的?
您实际输入的是0~5v的方波还是±2.5V的方波?