This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
利用OPA657搭建了一个宽带宽的积分器电路
从Bode图中可以看出在100Hz到1MHz有明显的积分效果,仿真结果也证明了这一点
但是在实际电路中,效果如下图
不知道问题出在哪里,请帮忙解决
积分电路电容是跨接在反向输入端和输出端之间,您这个电路形式设计的就是这样的吗
看您的实际电路,输入信号经R1和C1低通滤波电路输入至运放反向输入端,而RC滤波器的截止频率大概为81HZ,输入至运放的有效信号基本上都被衰减至0了,这一点不知道是不是您需要的?
您实际输入的是0~5v的方波还是±2.5V的方波?