Other Parts Discussed in Thread: OPA462
据OPA454的datasheet描述可以使用单电源供电,按照下图设计了PCB进行实验,输入与输出都是共地的,电源的也是共地的,电压放大倍数16倍
实验的结果如下
蓝色为100mv到3V的锯齿波输入,黄色为输出,输入还没有到最低点输出就饱和了。
请问以上现象是怎么引起的?该如何解决?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
1,实际应用V-确实接地的,接在板子的地
2,供电电压V+实际由DC-DC电源供电,是46V。按照您的说法,我这边确实应该要51V及以上供电才比较稳妥,但是实际的实验现象个人认为不是由于这个供电电压不够引起的。如果是因为供电电源不够引起的,应该是输出波形的峰值达不到。
3,实际上OPA454输入是200mV到3.3V的锯齿波,该现象是不是由于您提到的输入电压低于输入共模电压引起的?因为OPA454输入共模电压范围典型值是(V–) + 1.5V 至(V+) – 1.5V,而输入在1.5V左右就输出就出现了变化,即输出不在线性范围内了。
1、3V输入的话,16倍放大,最大输出应该是48V,但是看您的输出波形,最大是40V,已经饱和了
2、单电源供电的话,建议您输入2.5V 以上的信号,增益小一些的设置以验证输出是否正常?
3、另外,以上波形测试时,输出端是接的什么负载?断开负载测试看波形怎样?
您好,您的问题解决了没有,如果没有,您可以给出以下2点的情况吗
2、单电源供电的话,建议您输入2.5V 以上的信号,增益小一些的设置以验证输出是否正常?
3、另外,以上波形测试时,输出端是接的什么负载?断开负载测试看波形怎样?
在上面示波器第一种情况中,输入信号如下红色圈内部分,这部分信号频率是比较高的,您可以测量时拉开查看其变化率,运放在输入大信号时需要考虑其压摆率SR是否满足其要求,若不满足要求,输出信号就会失真,SR=2*π*f*VPP,f就是信号频率,VPP是输出信号峰峰值,OPA454的SR是13 V/µs。您测量的第一种情况应该是SR不足造成的