我们想使用INA226测量输入的电压和电流。我们的电源输入到隔离电源模块,我们现在想要测隔离电源模块前端(也就是电源输入口)的电压和电流,输入的电压差是30V,电流采用采样电阻来测量。请问INA226可以用于测量隔离电源的前级的电压和电流吗?
如果不能,麻烦推荐一下可以测量隔离电源前级的方案。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们想使用INA226测量输入的电压和电流。我们的电源输入到隔离电源模块,我们现在想要测隔离电源模块前端(也就是电源输入口)的电压和电流,输入的电压差是30V,电流采用采样电阻来测量。请问INA226可以用于测量隔离电源的前级的电压和电流吗?
如果不能,麻烦推荐一下可以测量隔离电源前级的方案。
这种不可以测量,因为INA226对电压的测量其参考基准是INA226的GND,而在您使用的电路中,被测回路的地和INA226的GND是隔离的,因此无法测量。
目前,我还不知道TI有哪款产品可以实现这种测量,我再去确认下
您好,我查到了TI的隔离式放大器,可以对电压信号进行隔离测量,但是对GND的输入电压范围最大 为±12V,无法满足您的要求。
TI应该没有芯片可以实现您需要的这种测量,另外您这种测量连线(即将INA226的GND和隔离后的地连一起而输入信号是隔离前的信号)使得隔离电源就失去了隔离作用。
有一种建议就是将INA226的供电电源使用DCDC隔离前的电源,然后对输出的信号I2C使用I2C 隔离器,然后再与后级电路相连