Part Number: THS3001EVM
Other Parts Discussed in Thread: THS3001
您好,我们遇到的问题单端加供电电压15V,供电电流50mA以上,芯片发烫,输出波形机型。增益为2,输入幅值范围在评估板上测试的。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: THS3001EVM
Other Parts Discussed in Thread: THS3001
您好,我们遇到的问题单端加供电电压15V,供电电流50mA以上,芯片发烫,输出波形机型。增益为2,输入幅值范围在评估板上测试的。

您好,
THS3001输入范围和输出范围都达不到电源轨,大概有2V的距离
在单电源15V供电时,输入信号范围大概为2V ~ 13V,输出信号范围也大概在这个范围,具体与负载大小有关
上图测试波形,您是输入幅值范围多少的信号测得的?

负载越大,输出电压范围越窄,看上面datasheet截图,在±5V供电时,RL=150Ω时,输出范围典型值是±3.2V;RL=1kΩ时,输出范围典型值是±3.3V;因此,供电电压一定的情况下,输出范围与负载有关;
因为,在单电源15V供电时,输入信号范围大概为2V ~ 13V,而您输入0.2-4V,因此有一部分输入信号不在THS3001输入范围内,使得输出异常。
在单电源15V供电时,您可以输入2V ~ 4V范围的信号,增益设置为3,这样输出为6~12V,使得输入输出都在THS3001的范围内,看下输出是否正常?