hi,
下图是我LMV331的应用电路,用于电池的ID检测;
VBAT_ID网络不接电池的电压是3.5-3.8V,接电池电压在2V-2.2V之间,VDD电压为3.3V;
另外在规格书中有看到推荐输入电压要比VCC低1.5V,我们供电使用的5V,最大输入是3.8V,请帮看下我的电路,看下是否有错误


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.