This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,
下图是我LMV331的应用电路,用于电池的ID检测;
VBAT_ID网络不接电池的电压是3.5-3.8V,接电池电压在2V-2.2V之间,VDD电压为3.3V;
另外在规格书中有看到推荐输入电压要比VCC低1.5V,我们供电使用的5V,最大输入是3.8V,请帮看下我的电路,看下是否有错误
您好,
LMV331的2脚不能通过电容接地,通过电容接地芯片是不能正常供电的,您将电容去掉,将GND pin直接接地,看是怎样的?
还有,您附的这个表格是从哪里看到的?
另外,5脚封装的话,1脚是IN+,3脚是IN-
下图的供电电压是耐压值还是常规工作电压,我们供电可能会波动到5.2V
LMV331的供电电压可以到5.5V