This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6629: LMH6629

Part Number: LMH6629


请问一下,谁能帮我看看我这个简单的放大电路为什么没有放大信号输出,在这里我用一个10k串1R进行电压信号分压模拟输入信号测试放大电路,在multisim仿真也是可行,而实际电路并不能正常工作!

  • 您好,LMH6629的电压范围为2.7V~5.5V,而您的电路中是+-5V供电,换成单电源为10V供电,超出了它的工作电压范围,所以是不能正常工作的。 如果在工作电压范围内验证的话,建议重新更换一片,防止由于过压导致的芯片损坏。

  • 你好,在你的指导下,我做了改变并且也重新焊了LMH6629,但是还是没有放大信号,只是有工作电压的直流信号出现在输出端,请问这是怎么回事?

  • 你好,在你的指导下,我做了改变并且也重新焊了LMH6629,但是还是没有放大信号,只是有工作电压的直流信号出现在输出端,请问这是怎么回事?

  •  你好!我想问一下LMH6629的工作电压范围是-0.5到6V吗?还是只要我能保证V+与V-之间的电压差值为之前你发的范围即可?不用考虑工作电压的数值?

  • 您好,不能参考这个绝对值,这个电气特性表格指的是芯片能承受的最大电压范围。 不代表的是功能性测试指标。

    每个芯片的电气参数需要参考”Recommended electrical characteristics”。所以对于LMH6629来说,5V供电的条件下,它的输入电压安范围为-0.3V~3.8V:

  • 你好!我想问一下LMH6629供电有要求吗?比如V+为+5V,V-为0V,或者V+为8V,V-为3V等等如此,只要我保证V+V-之间的压差不超过范围即可吗?

  • 是的,只要不超过正负电源差就可以,比如V+为+5V,V-为0V是可行的,但或者V+为8V,V-为3V不可行,这样正负压差为11V,而LMH6629的最大电压不超过5.5V的哈。