This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA567: 麻烦问一下该放大器的输出电流稳定度是多少啊?手册里怎么没找到呢

Part Number: OPA567


我想用OPA567做一个LED驱动电路,但是没找到该放大器的输出电流稳定精度,感谢大家

  • 您好,

    OPA567 输出摆幅在供电轨300mV范围内,输出电流为2A,较小的负载允许输出摆动更接近轨道。OPA567 输出电流与外接负载有关,或者说与发热功率有关,发热功率越大(管压降VS – VOUT)越大,输出电流能力越小,具体见 datasheet figure7 和 figure8

  • 谢谢您的回复,我了解运放的最大摆幅是300mV,但是我想知道的是这个运放的输出电压不稳定度是多少,因为我要用它作驱动电路,需要知道运放在5V供电下的输出电压稳定程度

  • OPA567输出电压稳定度主要与供电电压、负载、输入信号有关,OPA567输出级是class AB输出,它有上下2个输出晶体管,输出晶体管有输出阻抗,它与频率有关,如下截图,直流情况下是0.1Ω,那么输出电压VO就是供电电压VS与输出阻抗RO和外接负载RL的欧姆定律,即VO=VS*RL/(RL+RO)

    请注意OPA567有一个安全工作区(SOA),即我上一条回复中的截图,从根本上说它与运放的发热功耗有关;

    另外,我知道TI 有专门的(汽车、背光、照明、RGB、显示等) LED 驱动器,您也可以考虑使用专用的LED 驱动器,如下筛选链接:

    https://www.ti.com.cn/zh-cn/power-management/led-drivers/products.html

  • 好的好的,感谢感谢