This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BUF802RGTEVM: BUF802使用问题

Part Number: BUF802RGTEVM
Other Parts Discussed in Thread: OPA140, BUF802

根据IC推荐的应用电路制板焊接试验,连接该电路发现对测试产品(Oscillator)的消耗电流有较大的增加,如图是跟接泰克的P6243探头的电流比对。请问对此电路有什么办法可以改善此现象或推荐别的放大器?

希望接上放大电路对产品的影响(消耗电流,上升下降时间,占空比等等)尽量小,因为不同规格的Oscillator,其供电电压范围从0.8V到5V,消耗电流范围从10uA到30mA,频率范围也从32K到1.2GHz,所以要求还是蛮高的。

  • 您好,

    OPA140的输入衰减因子R4、R9、R13,在选择的时候我认为可以适当再加大些,这样可以进一步减小对被测产品的电流消耗方面的影响。

  • 感谢回复!

    根据回复信息,通过实验,将输入衰减因子的阻值加大(原为1M,现为10M),发现测得高频产品的电流值没有改善。即使是5V的产品,1M的负载,电流也只有5uA,我认为这个影响应该不是主要的。

    目前低频段电流加幅几乎可以忽略,频率越高,加幅越大。所以我怀疑是不是BUF802的main path的负载(电容)所致。

    另外,该IC供电电压+/-5V时,输出是不是有钳制,高电平不会超过3V?测试5V供电的Oscillator时,测得的输出波形会失真,低电平会抬高。见图

    以上问题还请帮忙回复解决,谢谢。

  • DEMO板TI推荐的模式为B,如果使用model A,图一中H1-H5回路的元件选择有什么需要考虑或推荐的吗?

  • 我再看一下这个电路,请耐心等一下

  • BUF802的输出不是轨至轨输出,查看下面输出摆幅表格,在输出高电平时(25℃时),距离电源轨至少1.8V,因此,5V供电时,输出约3V是正常的;

    我认为应该不是BUF802的main path的电容所致,因为它这个电容形成了不输入信号的负载;

    有没有可能是阻抗不匹配造成的?测试产品(Oscillator)输出是怎样连接到上述电路的?连接线是否比较长,其寄生电容是多少?或BUF802输入端是否存在寄生电容?

    关于model A,抱歉,我没找到关于其元件选择的相关资料