Part Number: AMC1100
Hi,
注意到AMC1100的SOP8封装是9.50 mm × 6.57 mm 大小的,但是有很多其他的SOP8封装的是 5.85mmx7.5mm, 比如NSI1300,
我的问题是为什么会出现同样的SOP8封装,但是尺寸不一样?
谢谢
Eason
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AMC1100
Hi,
注意到AMC1100的SOP8封装是9.50 mm × 6.57 mm 大小的,但是有很多其他的SOP8封装的是 5.85mmx7.5mm, 比如NSI1300,
我的问题是为什么会出现同样的SOP8封装,但是尺寸不一样?
谢谢
Eason
Hi Amy,
感谢回复,你可以在以下网站找到NSI1300:
https://www.sekorm.com/doc/2640158.html
但是我更想弄清楚TI的封装命名逻辑,在TI封装查找网站: https://www.ti.com.cn/packaging/cn/docs/searchtipackages.tsp?packageName=SO
输入SOP 和8 Pin脚封装,可以得到如下结果:

这几个尺寸差异巨大的封装都被归到了SOP8 下面,虽然TI的封装名称差距很大,但是在有些数据表中仍会显示SOP8封装。 所以我想问,我们TI在对封装进行分类时,是怎么来定义封装系列的? 比如,为什么上图这四个封装属于SOP8系列?
谢谢!
Eason