This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1100: 关于 SOP8 封装

Part Number: AMC1100


Hi,

注意到AMC1100的SOP8封装是9.50 mm × 6.57 mm 大小的,但是有很多其他的SOP8封装的是 5.85mmx7.5mm, 比如NSI1300,

我的问题是为什么会出现同样的SOP8封装,但是尺寸不一样?

谢谢

Eason

  • 您好,

    我没找到NSI1300的datasheet ,我不知道5.85mmx7.5mm中的这两个参数具体指什么参数;

    AMC1100的SOP封装尺寸如下截图,可能每个厂家的封装尺寸定义不一样。不管哪个厂家的产品,在第一次使用时,建议都仔细确认所使用封装尺寸与datasheet一致,然后再加入自己的封装库中,以备以后设计时循环使用。

  • Hi Amy,

    感谢回复,你可以在以下网站找到NSI1300:

    https://www.sekorm.com/doc/2640158.html

    但是我更想弄清楚TI的封装命名逻辑,在TI封装查找网站: https://www.ti.com.cn/packaging/cn/docs/searchtipackages.tsp?packageName=SO

    输入SOP 和8 Pin脚封装,可以得到如下结果:

    这几个尺寸差异巨大的封装都被归到了SOP8 下面,虽然TI的封装名称差距很大,但是在有些数据表中仍会显示SOP8封装。 所以我想问,我们TI在对封装进行分类时,是怎么来定义封装系列的? 比如,为什么上图这四个封装属于SOP8系列?

    谢谢!

    Eason