This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近一个项目用到了可调增益放大器THS7002,样板焊接完成后上电测试,不一会就发现THS7002发热严重,串入电流表测量该IC的电流达到了42mA,检查了电路设计和焊接均未发现问题。
重新找了一块空板,只焊接一个THS7002的IC,用可调电源加上24V电压到IC上,分别测量第8脚(PREAMP VCC+)电流13mA 和第21脚(PGA VCC+)28mA。
查了一下规格书,PGA ICC的最大静态电流在正负15V的电压下每通道7mA,THS7002内部有两个PGA,最大电流应该在14mA以内,而PGA的实测电流是28mA,达到规格书的两倍,请问这是什么原因?
下面截图是THS7002双电源供电时静态电流随温度变化曲线,在同一温度下,供电电压越高,静态电流是稍微增大的。
您的意思是说当输入电压为 ±10V 时,VCC+的电流就会达到20mA以上?您测试了几块板子是这种情况,您可以把您测试的具体连线的电路附上吗?
抱歉,我上一条回复中将您说的-10V输入错误的理解为了供电电压为±10V;
我是这样理解的,在双电源供电时,如果输入信号不为0,那么运放内部一些管子就会导通,就会产生电流消耗;如果输入信号为0,那么输出信号对地输出也为0(排除运放同向和反向因工艺问题不对称产生的误差),运放内部一些管子就不会导通,也就不消耗电流。
感谢您对电路做了仿真。在您的仿真电路中,也可以看到,在输入-10V时,反向输入端从运放也抽取了一部分电流,如您测出的-8.76480mA,这部分电流就是从供电端输入的,也可以看到VCC+端电流为10.0219mA,比输入信号为0V时多了5多mA。