This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS7002: 发热严重,空载电流达到了40mA

Part Number: THS7002
Other Parts Discussed in Thread: THS7001

最近一个项目用到了可调增益放大器THS7002,样板焊接完成后上电测试,不一会就发现THS7002发热严重,串入电流表测量该IC的电流达到了42mA,检查了电路设计和焊接均未发现问题。

重新找了一块空板,只焊接一个THS7002的IC,用可调电源加上24V电压到IC上,分别测量第8脚(PREAMP VCC+)电流13mA 和第21脚(PGA VCC+)28mA。

查了一下规格书,PGA ICC的最大静态电流在正负15V的电压下每通道7mA,THS7002内部有两个PGA,最大电流应该在14mA以内,而PGA的实测电流是28mA,达到规格书的两倍,请问这是什么原因?

  • 您好,

    PREAMP的电流是正常的,每通道大概为7mA;

    PGA  的静态电流有些偏大,每通道大概5mA,不知道是否与PowerPAD的连接有关,在您的电路中PowerPAD是否通过过孔接地,像datasheet 中 general PowerPAD design considerations部分描述的那样

  • 感谢你的分析,Power PAD确实没有焊,把Power PAD焊接正确后,温度略有下降,但PGA电流没有任何变化,仍然超过规格书一倍。帮忙看下还有什么地方会影响PGA的静态电流?

  • 给THS7002的PGA提供 (VCC+ + VCC- )/2的输入电压,即供电电压的中间值,VH和 VL也提供合适的钳位电压,使PGA的输入和输出都在正常范围内,然后悬空输出,测试PGA电流是多少?

  • 按照你的描述,PGA的VCC+和VH接+12V,PGA的VCC-和VL接-12V,输入接地,悬空输出后测试,VCC+的电流降到9.3mA。经过反复研究和测试,发现PGA的电流和输入电压是相反的关系,即便输出悬空。当输入电压增高时,VCC+电流会下降,输入电压下降时,VCC+电流会升高。当输入电压下降到-10V时,VCC+的电流就会达到20mA以上。请问这是什么原因?

  • 下面截图是THS7002双电源供电时静态电流随温度变化曲线,在同一温度下,供电电压越高,静态电流是稍微增大的。

    您的意思是说当输入电压为  ±10V  时,VCC+的电流就会达到20mA以上?您测试了几块板子是这种情况,您可以把您测试的具体连线的电路附上吗?

  • 是的,我测试了三片都是这样。刚才从TI官网下载了THS7001的仿真模型,用ORCAD进行了仿真,仿真电路如附图。

    在+/-12V供电的情况下:0V输入的电流是4.97mA,-10V输入的电流升到了10.02mA. THS7002内置了两个THS7001,THS7002的电流应该是THS7001的两倍。实测值和仿真结果是一致的。

  • 抱歉,我上一条回复中将您说的-10V输入错误的理解为了供电电压为±10V;

    我是这样理解的,在双电源供电时,如果输入信号不为0,那么运放内部一些管子就会导通,就会产生电流消耗;如果输入信号为0,那么输出信号对地输出也为0(排除运放同向和反向因工艺问题不对称产生的误差),运放内部一些管子就不会导通,也就不消耗电流。

    感谢您对电路做了仿真。在您的仿真电路中,也可以看到,在输入-10V时,反向输入端从运放也抽取了一部分电流,如您测出的-8.76480mA,这部分电流就是从供电端输入的,也可以看到VCC+端电流为10.0219mA,比输入信号为0V时多了5多mA。

  • 看来IC的电流确实会随着输入信号的变化而变化。感谢你的协助分析。