我是用THS4304搭建了一个简单反相比例放大器,我需要使用单电源供电,并且电压范围在0~5V用于ADC采样。
问题1:在我按照文档中的电路,在正相端接入VREF,它的输出范围在截至到了VREF~4V,但是我希望它的范围在0~5V。

问题2:于是我将正相端直接接地,放大后的信号变得很小(几乎缩小了1000倍),我不知道这是为什么。

问题3:另外,能够给我推荐一个1.5G Hz左右的带宽(1.5倍增益),单电源供电,并且能够使得输出电压范围在0~5V的运放吗?
感谢您的帮助!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我是用THS4304搭建了一个简单反相比例放大器,我需要使用单电源供电,并且电压范围在0~5V用于ADC采样。
问题1:在我按照文档中的电路,在正相端接入VREF,它的输出范围在截至到了VREF~4V,但是我希望它的范围在0~5V。

问题2:于是我将正相端直接接地,放大后的信号变得很小(几乎缩小了1000倍),我不知道这是为什么。

问题3:另外,能够给我推荐一个1.5G Hz左右的带宽(1.5倍增益),单电源供电,并且能够使得输出电压范围在0~5V的运放吗?
感谢您的帮助!
3、TI的放大器可以在下面链接筛选,网页左边是筛选条件,可以根据参数需求进行筛选:
https://www.ti.com.cn/zh-cn/amplifier-circuit/op-amps/products.html
在单电源供电中,如果需要输出0~5V,那么运放的输出需要摆到负的电源轨0V,即需要轨至轨输出到负电源轨0V,至于输出最大值5V,可以选择供电电压大于5V的运放,这样输出正轨达不到正电源轨也没关系,能达到5V就可以。但是我看了下GBW大于3GHZ的运放,没有满足要求的。因此,恐怕您需要双电源供电才可以。
关于带宽,高速运放会分小信号带宽和大信号带宽,这个主要是受压摆率SR的限制,因此找到一个运放后需再仔细看下带宽是否满足要求。
4、这应该是一个普遍现象,即使标注是轨至轨输出的运放,其输出也不能完全达到电源轨,只是比较接近电源轨而已。因为运放输出级的晶体管会产生一定的压降,如下图所示。