Part Number: XTR111
我使用xtr111进行压流转换,输入是0~3.3V,输出理论上应该是0~10mA。
但是我测量之后发现当供电电压是12V,排针J1的3、4之间接入4KΩ的电阻,输入电压是1V时(电流理论输出值是3.33mA),R12(15Ω)上的压降大约50mV,,降低输入电压后,R12上的压降也基本符合计算的理论电流值与其阻值的乘积。但是升高输入电压,SET引脚上的压降,即R10和R14一共的压降,变化不明显,输入2V时,SET处电压才升高一点,可是依然比较接近1V。R11右端的输入电压也是这种情况,比较接近1V。
4kΩ电阻上一直只有大约0.4或0.5V的压降。EF引脚上的电压是4.5V。
感觉电流好像放大了10倍,但没有实现恒流输出。