This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA849: 输出信号严重偏移

Part Number: INA849

用INA做小信号放大用,发现当输入信号较大时,输出相对基准电压偏移非常多。
当输入信号约为25mV时,输出以基准电压(2.5V)为中心摆动,如下图1
当输入信号约为0.5V时,输出偏移基准电压(2.5V)数伏之多,如下图2
请帮分析可能的原因是什么,电路参数说明:增益为300,供电为正负10V,基准电压为2.5V
图1
图2