Part Number: LMC6084
Other Parts Discussed in Thread: LMC6082
传感器为光电二极管,分别使用LMC6082和LMC6084组成了电流电压转换电路。正电源10V,负电源-3V。调试时将负电源从-1V调至-4V,LMC6084的几路信号基线从0.5V跳至负电源电压,继续跳至20mV以上且有增大趋势。LMC6082的几路信号基线则正常。很是困惑,换了一块LMC6084芯片,问题依旧。


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
有可能是布线的问题,运放的输入和输出信号都是敏感信号,应该注意其他信号对它们的影响,在这里主要是供电电源信号。在板子其他部分不知道是否有离它们比较近的高频信号或电源信号,也请注意下。
调试时将负电源从-1V调至-4V,LMC6084的几路信号基线从0.5V跳至负电源电压,继续跳至20mV以上且有增大趋势
这个过程是将负电源调至一个固定电压后测量的运放输出,是吗?
运放的供电电源是什么电源?线性电源还是开关电源?与LMC6082是使用的同样的电源IC产生的吗?
LMC6084上的电压跟随器输出是怎样的呢?用示波器测量下其输出,看是否存在波动?
也不能排除信号间的相互影响,为排除LMC6084上3路信号间的影响,您可以仅连接一路光电二极管,其他接成电压跟随器形式,然后测试这一路光电二极管的输出信号吗?测试信号时,建议用示波器测量,这样可以更直观的反应信号的质量