INA821在5V单电源供电或者12V单电源供电时,没有输出信号,或者输出与输入没有任何的关联
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
被测回路与INA821不共地吗?我看电路图中INA821的地是AGND,被测回路是GND;被测回路需与INA821共地,否则的话,无法定义INA821的共模输入电压;
INA821的输出公式是:
即放大的是V+IN和V-IN的差值,因此单电源供电时,V+IN电压大于V-IN电压,输出才能正常输出,否则的话,输出的是负值,单电源供电时,INA821无法输出负值。或者需要通过VREF管脚抬高INA821的输出电压,在输出负的电压值时,其绝对值小于VREF电压,这样输出电压加上VREF电压也是正值,也可以正常输出;
另外,注意在单电源供电时,其输出幅值范围不能完全达到电源轨,距离地电平有0.15V的距离,也就是说最小输出电压是0.15V,应用时设计的最小输出电压应大于0.15V:
如上截图,我再附一次如下,仪表运放有共模输入电压要求,INA821一般来说至少要在(V–) + 2 至 (V+) – 2V,供电电压是单电源12V的话,那么输入共模电压范围就是2V 至10V,具体范围还取决于输入电压、增益和Vref电压,可以使用Analog Engineers Calculator这个工具来设计,如下链接:
https://www.ti.com/tool/ANALOG-ENGINEER-CALC?keyMatch=ANALOG%20ENGINEERS%20CALCULATOR
使用方法可点击Help按钮查看;
上图中输入共模电压是[15V/(0.003Ω+20Ω)]*0.003Ω/2,这个值小于2V,因此输出会饱和;
关于您的应用电路,电流是1A的话,流过0.003Ω的采样电阻,电压是3mV,也不满足仪表运放的输入共模电压要求,因此输出会饱和;
如果需要使用单电源供电的话,那么需要给输入端加一个共模电压,使采集信号满足共模输入电压范围;