Other Parts Discussed in Thread: THS3096, THS3092
目前需求是:
把输入的TTL信号 0-5V(2kHz,上升下降沿均在7ns以内)
通过一个双轨运放,做成反向比例放大电路,输出在0- -10V之间 (上升沿、下降沿均小于3ns)
因此算出SR最好在5kV/us 支持±15V供电的高速运放
想问下推荐的型号有吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,5000V/us的高速器件,筛选出来只能考虑电流反馈运放了。
双路的话,宽电压范围的可以考虑THS3092,THS3096,您再看下它的数据手册,确认下其他电气参数,比如带宽,噪声,封装等是否也符合您的要求.