This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS4032: 寻求一款高SR的正负压供电运放

Part Number: THS4032
Other Parts Discussed in Thread: THS3096, THS3092

目前需求是:

把输入的TTL信号 0-5V(2kHz,上升下降沿均在7ns以内)

通过一个双轨运放,做成反向比例放大电路,输出在0- -10V之间 (上升沿、下降沿均小于3ns)

因此算出SR最好在5kV/us 支持±15V供电的高速运放

想问下推荐的型号有吗