This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA992: 能否扩压使用,如何判断运放是否满足扩压使用条件

Part Number: OPA992

如图,这样使用OPA992作为扩压正确吗

  • VF 3=110V,VF 2=106V ?

    不能哦,OPA992的供电电压2.7V~40V双电源+-1.25V~+-20V. 不论以什么方式,超过这个电压范围运放就有可能永久性损坏。

  • 感谢你的回复

    你说的这个供电电压2.7V~40V双电源+-1.25V~+-20V指的是电源两端的压差,而且是运放在标准状态下的使用,我想请教的是运放的扩压的问题,所以不一样

  • 您好,对于OPA992的供电电压以及输出电压,我看到您使用TINA提高到110V输出,作用在V+ 和V-的电压也在110·和106V左右,这个是不可以的。虽然压差为4V,但是也不满足它可以承受的电压值。

    OPA992的正常工作条件下,V+的电压范围为1.25~20V,V-的电压范围为-1.25~-20V。 如果V-接GND的话,V+ 的电压范围就是2.7~40,超过这个范围运放会损坏。