如图,这样使用OPA992作为扩压正确吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
VF 3=110V,VF 2=106V ?
不能哦,OPA992的供电电压2.7V~40V双电源+-1.25V~+-20V. 不论以什么方式,超过这个电压范围运放就有可能永久性损坏。
您好,对于OPA992的供电电压以及输出电压,我看到您使用TINA提高到110V输出,作用在V+ 和V-的电压也在110·和106V左右,这个是不可以的。虽然压差为4V,但是也不满足它可以承受的电压值。
OPA992的正常工作条件下,V+的电压范围为1.25~20V,V-的电压范围为-1.25~-20V。 如果V-接GND的话,V+ 的电压范围就是2.7~40,超过这个范围运放会损坏。