This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
这个120V供电范围是决对最大额定值,是保证芯片不被损坏的范围。推荐的工作条件中的供电范围是保证芯片电气特性的范围,一般不建议超过推荐的工作条件。
您说的空载是输出电流为0吗?您可以附上电路图吗?107V的供电电压,静态电流是3.2mA,静态功耗是342mW,芯片温升与PCB散热设计也有关,您说的发烫大概温度是多少?
所附电路中使用了3个 OPA454,我看前两个电路是一样的,最后一个反向输入是5V_E,反向放大约18倍,您这里5V_E是5V电压吗?这样反向放大18倍是-90V,超出了供电范围输出会截止的,这是您期望的吗?
如果功能正常的话,应该是PCB散热的问题,如果过热的话会进入thermal shutdown状态:
是的,需要将PAD接至V-,这里没问题;
关于散热,主要是降低热阻θJA,它受安装技术和环境的影响。空气循环度和导热物体表面的连接热阻、PCB板元器件的排列紧密度都会影响芯片对环境的散热。可以加大覆铜面积和PCB迹线宽度等增加散热,数据手册Figure 88有电路板铜面积与热阻的关系曲线,铜面积增加到大约0.5 in2可降低热阻,超过0.5 in2时,继续改善的作用不明显。有关散热的更多信息,请查看SBOA021:https://www.ti.com.cn/cn/lit/an/sboa021/sboa021.pdf