Part Number: INA199
大家好!
我们有个项目用到了INA199A1这款放大器,但在使用过程中发现不需要50倍这么高的放大倍数,于是在IN-引脚断开与Load-的连接,在IN-与Load-串接一个51K的电阻,如下图所示。
理论上算得的放大倍数G = 1 + R1/(R3+R5) = 1 + 1MΩ/(20KΩ+51KΩ) ≈ 15倍。
但是在实际测量中,发现这样的接法放大倍数约只有3倍,不知是何原因,请指教,谢谢!

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.